Compare selected products
Product code
Removable battery
Battery capacity
A measure of the charge stored by the battery. Determined by the mass of active material contained in the battery.
Call divert
Call hold
Caller ID
The name and/or number of the caller comes up on screen when they ring the phone. You also send your caller ID when you call someone else unless you choose to deactivate it.
Conference call
Call waiting
Speed dialling
Call timer
Rear camera field of view (FOV) angle
Second rear camera aperture number
Third rear camera aperture number
Rear camera pixel size
Second rear camera pixel size
Third rear camera pixel size
Second rear camera field of view (FOV) angle
Rear camera resolution
Third rear camera field of view (FOV) angle
Optical zoom
Indicates the optical zoom capacity, which is the number of times that the picture can be enlarged with the optics of the camera.
Digital zoom
Indicates the digital zoom capacity, the number of times that the picture is enlarged thanks to digital technology.
Front camera type
Indicates the type of the camera at the front of the product, dual or single.
Front camera aperture number
Front camera pixel size
Front camera field of view (FOV) angle
Rear camera flash
Whether or not the rear camera features its own flash.
Flash type
Video capture resolution (max)
Resolution at capture speed
Video recording modes
Rear camera aperture number
Front camera resolution (numeric)
Third rear camera resolution (numeric)
Video recording
Recording moving visual images.
Night mode
Self-timer
Multi-shot
Geotagging
Second rear camera resolution (numeric)
Video stabilizer
Image stabilizer
This camera function compensates for slight shaking movements caused by an unstable position and ensures smooth footage even in suboptimal conditions.
Face detection
Zoom capability
The amount that the camera lens can zoom.
Auto focus
Device focusing a camera or other piece of equipment automatically.
Rear camera sensor size
Rear camera resolution (numeric)
The resolution of the images produced with the rear camera, given in MP (megapixel. 1 MP = 1 million pixels).
Rear camera type
Indicates the type of the camera at the back of the product, dual or single.
Extremities SAR (EU)
Body SAR (EU)
SAR stands for Specific Absorption Rate which is the unit of measurement for the amount of radio frequency (RF) energy absorbed by the body when using mobile equipment.
Head SAR (EU)
SAR stands for Specific Absorption Rate which is the unit of measurement for the amount of radio frequency energy absorbed by the head when using mobile equipment.
Form factor
The shape or design of the product.
Protection features
Physical effects from which the product is protected e.g. water resistant, crash proof.
International Protection (IP) code
The IP code classifies and rates the degree of protection provided against the intrusion (including body parts such as hands and fingers), dust, accidental contact, and water by mechanical casings and electrical enclosures. It is published by the International Electrotechnical Commission (IEC). The digits (characteristic numerals) indicate conformity with the conditions summarized in the tables below. Where there is no protection rating with regard to one of the criteria, the digit is replaced with the letter X. an electrical socket rated IP22 is protected against insertion of fingers and will not be damaged or become unsafe during a specified test in which it is exposed to vertically or nearly vertically dripping water. Another example is the Sony Xperia Z Ultra, one of the first cellular phones to be IP-rated; it is rated at IP58 and marketed as "dust resistant" and can be "immersed in 1.5 meter of freshwater for up to 30 minutes".
Colour name
Product colour
The colour e.g. red, blue, green, black, white.
Screen shape
Display diagonal
Size of the display for this product, measured diagonally, usually in inches.
Gorilla Glass version
Display technology marketing name
Pixel density
Touchscreen type
There are a variety of touchscreen technologies that have different methods of sensing touch, including resistive and capacitive.
High Dynamic Range (HDR) technology
High Dynamic Range (HDR) supported
Touch technology
Technology of touch sensetive screen e.g. dual-touch.
Maximum refresh rate
Native aspect ratio
The aspect ratio is the ratio of the width of an image to its height. The native aspect ratio is the one which the projector/display is particularly designed for. Images shown in native aspect ratio will utilize the entire resolution of the display and achieve maximum brightness. Images shown in other than native aspect ratio will always have less resolution and less brightness than images shown in native aspect ratio.
Display number of colours
Display resolution
The number of distinct pixels in each dimension that can be displayed. It is usually quoted as width × height, with the units in pixels: for example, "1024 × 768" means the width is 1024 pixels and the height is 768 pixels. The higher the number of pixels, the sharper the image.
Display glass type
Rounded display corners
Panel type
Harmonized System (HS) code
Short Message Service (SMS)
Multimedia Messaging Service (MMS)
Multimedia Messaging Service (MMS) is a standard way to send messages that include multimedia content to and from a mobile phone over a cellular network
Instant messaging (IM)
Chat
E-mail
Text prediction system
Speakers
Supported video modes
The video modes that can be displayed by the device.
Audio system
System used to play music or speech.
Audio formats supported
The audio formats which this device or software can read/use e.g. MP3, MP4.
Video formats supported
The type of video formats that can be used by this device.
Image formats supported
The type of image files that the device can use/display e.g. gif, JPEG (jpg).
GPS (satellite)
Global Positioning System (GPS) is a space-based satellite navigation system that provides location and time information in all weather conditions, anywhere on or near the Earth where there is an unobstructed line of sight to four or more GPS satellites. The system provides critical capabilities to military, civil and commercial users around the world. It is maintained by the United States government and is freely accessible to anyone with a GPS receiver.
Assisted GPS (A-GPS)
Assisted GPS, generally abbreviated as A-GPS, enhances the startup performance of a GPS satellite-based positioning system. It is used extensively with GPS-capable cellular phones as its development was accelerated by the U.S. FCC's 911 mandate making the location of a cell phone available to emergency call dispatchers.
GLONASS
BeiDou
Galileo
Wi-Fi positioning
Position location
Whether the navigation system can locate the phone's position.
SIM card capability
How many SIM cards the device can hold.
3G standards
Near Field Communication (NFC)
Mobile network generation
SIM card type
2G standards
4G standard
Wi-Fi
Popular technology that allows an electronic device to exchange data or connect to the internet wirelessly using radio waves.
Wi-Fi standards
The type of wireless local area network (LAN). It can be ad-hoc, where units in a network communicate peer-to-peer, or Infrastructure, where units communicate with each other via an access point A LAN interconnects computers in a small area e.g. home, school or office.
Bluetooth
Bluetooth is a low-power radio technology developed to replace the cables and wires currently used to link or connect electronic devices such as personal computers, printers, and a wide variety of handheld devices including mobile phones. Because it uses radio-wave connectivity, a Bluetooth-enabled device has a constant, established connection to whatever browser it uses. This saves the user the trouble of logging on to check for emails or news updates, for example.
Bluetooth version
The type of bluetooth technology in the product e.g. Bluetooth Smart (v4.0).
3G bands supported
Tethering (modem-mode)
Wi-Fi Direct
MIMO
Touchscreen
A screen of a laptop, smartphone, etc., that responds to touch so you can control the interface using your fingers.
SIM card ejector pin
AC adapter included
Quick start guide
Instructions, either online, as a computer program or in paper form, to allow you to set up and start using the product quickly.
Cables included
Themes
Video call
Simultaneous video and audio signals to enable people to talk to and see each other in real time.
Fast charging
Wireless charging
Fingerprint reader
A scanner used to identify a person's fingerprint for security purposes. After a sample is taken, access to a computer or other system is granted if the fingerprint matches the stored sample. A PIN may also be used with the fingerprint sample.
Face recognition
Personal info management (PIM)
You can use your device to manage your information and your time.
Speakerphone
Device has a microphone and loudspeaker provided separately from those in the handset. This device allows multiple persons to participate in a conversation. The loudspeaker broadcasts the voice or voices of those on the other end of the telephone line, while the microphone captures all voices of those using the speakerphone.
Flight mode
Personalization
Support for contact groups
Microphone mute
Vibrating alert
USB On-The-Go support
ANT+ enabled
USB version
Universal Serial Bus (USB) is an industry standard developed in the mid-1990s that defines the interface used for connection, communication and power supply between computers and electronic devices. Every new version - for example 1.1, 2.0, 3.0 - is much faster than the previous one.
USB port
The device features a socket into which a USB cable can be plugged.
USB connector type
The type of USB connector/port that this product has.
Cores frequencies
Processor model
The model number for the processor in a computer.
Processor family
A family of processors is a group of processors produced by one company over a short period of time e.g. Intel Pentium processors.
Processor lithography
The process which is performed by the processor e.g. CPU (Central Processing Unit).
Processor cores
The number of central processing units ('cores') in a processor. Some processors have 1 core, others have 2 (e.g. Intel Core Duo) or more (e.g. the Intel Xeon E7-2850 has 10 cores).
Processor frequency
The speed that the microprocessor executes each instruction or each vibration of the clock. The CPU requires a fixed number of clock ticks, or cycles, to execute each instruction. The faster the clocks rate, the faster the CPU, or the faster it can execute instructions. Clock Speeds are usually determined in MHz, 1 MHz representing 1 million cycles per second, or in GHz, 1 GHz representing 1 thousand million cycles per second. The higher the CPU speed, the better a computer will perform.
Accelerometer
Ambient light sensor
Gyroscope
Orientation sensor
The device e.g. smartphone, tablet uses gravity to sense whether it should be displaying in portrait or landscape mode.
Barometer
Geomagnetic sensor
Hall sensor
Proximity sensor
Virtual assistant
Depending on the make of the device, a different application is pre-installed that can understand voice commands and complete tasks for a user, e.g. Apple Siri, Amazon Alexa.
Google applications
App distribution platform
Operating system installed
Type of operating system on a device e.g. IOS on Apple devices, Android for mobile devices.
Platform
Description of a technology platform including a processor, chipset, platform software and wired networking capabilities.
Compatible memory cards
Types of memory cards which can be used with this product.
RAM capacity
RAM type
The type of RAM (random access memory) inside the device e.g. DDR3.
Internal storage capacity
The amount e.g of data which can be stored inside the device.
Maximum memory card size
The maximum size of memory card that can be used with this device.
USB mass storage
Subscription type
The type of cellular connection subscription.
Repairability index
Weight
Weight of the product without packaging (net weight). If possible, the net weight is given including standard accessories and supplies. Please note that sometimes the manufacturer leaves out the weight of accessories and/or supplies.
Height
The measurement of the product from head to foot or from base to top.
Depth
The distance from the front to the back of something.
Width
The measurement or extent of something from side to side.