The Central Processing Unit (CPU) or (micro) processor is the part of a computer where most calculations take place. In terms of computing power, the processor is the most important element of a computer system, so the performance of a computer is highly dependant on the performance of the processor. For quite some time the performance of a processor has been determined by the number of MHz the clock speed was, but nowadays clock speed doesn't have so much to do with the speed of the processor anymore. One of the best ways to compare different kinds of processors, is to look up benchmarks on the internet. Please be careful to buy a processor that is compatible with your motherboard, i.e. fits in the right socket.
Release date: 22 Dec 2007
Info modified on: 27 Jun 2009 01:49:44
Product views: 13052
This statistic is based on the
6861
using ecommerce sites (eshops, distributors, comparison sites, ecommerce ASPs, purchase systems, etc) downloading this ICEcat data-sheet since
22 Dec 2007.
Only sponsoring brands are included in the free Open ICEcat content distribution as used by
6367
free Open ICEcat users .
The Central Processing Unit (CPU) or (micro) processor is the part of a computer where most calculations take place. In terms of computing power, the processor is the most important element of a computer system, so the performance of a computer is highly dependant on the performance of the processor. For quite some time the performance of a processor has been determined by the number of MHz the clock speed was, but nowadays clock speed doesn't have so much to do with the speed of the processor anymore. One of the best ways to compare different kinds of processors, is to look up benchmarks on the internet. Please be careful to buy a processor that is compatible with your motherboard, i.e. fits in the right socket.
Get powerful performance for your unique digital experience. It’s not just about email, Web browsing and word processing anymore. The AMD Athlon™ Single-Core processor gives you leading performance to go wherever your digital world takes you.
Specs
Alternatives
Options
Processor
Processor clock speed
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
2700 MHz
Processor family
The processor serie to which the processor belongs.
AMD Athlon 64
Processor socket
Socket AM2
Box
Processor
L2 cache
The CPU cache (Level 2 in megabyte) is a smaller, faster memory which stores copies of the data from the most frequently used main memory locations.
1 MB
Processor
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.